HAL I2C Overview

Introducing I2C

group I2C_Introduction

  • The I2C hardware abstraction layer provides a set of APIs to interface with the STM32 I2C (Inter-integrated circuit interface) peripheral.

  • It simplifies the configuration, initialization and management of I2C communication, by supporting various modes such as polling, interrupt, and DMA for efficient data transfer.

  • This abstraction layer ensures portability and ease of use across different STM32 series.

Module and files

The following diagram illustrates the I2C module and its associated files.

Module and files diagram

Component diagram

The following diagram illustrates the software components involved in the I2C module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.



@startuml
<style>
componentDiagram {
   arrow {
      FontSize 8
   }
}
</style>

title I2C Software Component Diagram

package "HAL" {
    [HAL_SERVICE]
    [HAL_I2C]
    [HAL_DMA]
}

package "Low Layer" {
    [LL_I2C]
    [CMSIS]
    [I2C Interrupt routine service]
    [DMA Interrupt routine service]
}

package "HW" {
    [STM32_HW]
}

[Appli] --> [HAL_I2C] : HAL I2C API
[Appli] <-- [HAL_I2C] : I2C callback
[HAL_I2C] --> [LL_I2C] : LL I2C API
[HAL_I2C] -r-> [HAL_DMA] : Configure DMA
[HAL_I2C] -l-> [HAL_SERVICE] : HAL_GetTick
[HAL_I2C] <-- [I2C Interrupt routine service]
[HAL_I2C] <-r- [HAL_DMA]:Half transfer complete\nTransfer complete\nError
[LL_I2C] --> [CMSIS]:I2C register def
[HAL_DMA] <-d- [DMA Interrupt routine service]
[STM32_HW] -u--> [I2C Interrupt routine service]: I2Cx Irq
[STM32_HW] -u--> [DMA Interrupt routine service] : DMA Channel Irq
[STM32_HW] <-u-- [LL_I2C] : I2C registers R/W
@enduml

Configuration table

The following table lists the configuration defines for the HAL I2C module, specifying their locations, default values, and descriptions:

group I2C_Configuration_Table

  1. Configuration inside the I2C driver

Software configuration defined in stm32h7pxx_hal_conf.h:

Preprocessor flags

Default value

Comment

USE_HAL_I2C_MODULE

1

Enable HAL I2C driver module

USE_HAL_I2C_REGISTER_CALLBACKS

0

Allow the user to define their own callback

USE_HAL_I2C_DMA

1

Enable DMA code inside I2C

USE_HAL_CHECK_PARAM

0

Enable runtime parameter check

USE_HAL_I2C_CLK_ENABLE_MODEL

HAL_CLK_ENABLE_NO

Enable the gating of the peripheral clock

USE_HAL_CHECK_PROCESS_STATE

0

Enable atomicity of process state check

USE_HAL_MUTEX

0

Enable semaphore creation for OS

USE_HAL_I2C_USER_DATA

0

Add a user data inside HAL I2C handle

USE_HAL_I2C_GET_LAST_ERRORS

0

Enable retrieval of last processes error codes

Software configuration defined in preprocessor environment:

Preprocessor flags

Default value

Comment

USE_ASSERT_DBG_PARAM

Not defined

Enable check param for HAL and LL

USE_ASSERT_DBG_STATE

Not defined

Enable check state for HAL