HAL I3C Overview ¶
Introducing I3C ¶
- group I3C_Introduction
-
The STM32 Hardware Abstraction Layer for I3C provides a comprehensive software interface to support the I3C communication protocol on STM32 microcontrollers. I3C (Improved Inter-Integrated Circuit) is an advanced, high-speed, and energy-efficient serial bus protocol designed to enhance and replace traditional I2C, offering features such as dynamic device management and higher data rates. While I3C maintains backward compatibility with many I2C devices, certain I2C features such as stretch mode are not supported. This HAL driver abstracts low-level hardware details, enabling configuration, data transfer, and interrupt handling, thereby accelerating development and ensuring robust, scalable embedded applications that leverage the full capabilities of the I3C bus.
Module and files ¶
The following diagram illustrates the I3C module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the I3C module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL I3C module, specifying their locations, default values, and descriptions:
- group I3C_Configuration_Table
-
¶
15. Software configuration ¶
15.1 Software configuration defined in stm32h7pxx_hal_conf.h: ¶
Preprocessor flags
Default value
Comment
USE_HAL_I3C_MODULE
1
Enable HAL I3C driver module
USE_HAL_I3C_REGISTER_CALLBACKS
0
Allow user-defined callbacks
USE_HAL_I3C_DMA
1
Enable DMA code inside I3C
USE_HAL_CHECK_PARAM
0
Enable runtime parameter check
USE_HAL_I3C_CLK_ENABLE_MODEL
HAL_CLK_ENABLE_NO
Enable the gating of the peripheral clock
USE_HAL_CHECK_PROCESS_STATE
0
Enable atomicity of process state check
USE_HAL_MUTEX
0
Enable semaphore creation for OS
USE_HAL_I3C_USER_DATA
0
Add user data inside HAL I3C handle
USE_HAL_I3C_GET_LAST_ERRORS
0
Enable retrieval of last process error codes
15.2 Software configuration defined in preprocessor environment: ¶
Preprocessor flags
Default value
Comment
USE_ASSERT_DBG_PARAM
Not defined
Enable check param for HAL and LL
USE_ASSERT_DBG_STATE
Not defined
Enable check state for HAL