HAL/LL drivers: security support ¶
The purpose of this chapter is to detail the security aspects in the HAL and LL drivers, based on
ARMv8 architecture
GTZC and RIF peripherals
RIF and GTZC HAL and LL drivers ¶
The unification of RIF and Trust Zone APIs is critical due to their similar usage within application layers, requiring consistent and harmonized interfaces for common features across both GTZC and RIF drivers. To address this, the architecture enforces attribute management through dedicated functions designed to ensure code portability across HAL and LL drivers. These functions must independently manage security, privilege, and lock attributes, as well as read and write access operations, with clear separation between items and attributes within function parameters. Additionally, function implementations must support both static configurations—such as establishing security attributes during application initialization by isolating resources between secure and non-secure, privileged and non-privileged domains—and dynamic configurations that enable attribute reconfiguration based on evolving application needs. This approach ensures a flexible, robust, and unified framework for security attribute management.
The following table lists the HAL and LL RIF and GTZC naming rules:
|
Concept wording |
HAL/LL RIF naming rule |
HAL/LL GTZC naming rule |
|---|---|---|
|
Block based sub-block |
RISAB: Resource isolation slave unit for address space protection (block-based) |
MPCBB: Memory Protection Controller Block-Based |
|
Illegal access sub-block |
IAC: Illegal access controller |
TZIC: Trust Zone Illegal access Controller |
|
Watermark sub-block |
RISAF: Resource isolation slave unit for address space protection (full version) |
TZSC_MPCWM: Memory Protection Controller - Watermark |
|
Periph Attr sub-block |
RIFSC: Resource Isolation Framework Security Controller RISC: Resource Isolation Slave Controller RIMC: Resource Isolation Master Controller |
TZSC: Trust Zone Security Controller |
|
Illegal access |
ilac |
|
|
Region |
region |
N/A |
|
Sub Region |
subregion |
|
|
Security |
Sec |
|
|
Non-Secure |
NSec |
|
|
Privilege |
Priv |
|
|
Read |
Rd |
|
|
Write |
Wr |
|
|
Address |
Addr |
|
|
Public |
Public |
N/A |
|
Non-Public |
NPublic |
N/A |
RIF and GTZ HAL driver’s architecture ¶
The HAL GTZ and RIF drivers must follow the rules below for naming, enumerations, function prototypes, and return values:
Enumerations:
Securable peripherals
typedef enum { HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_TIM2 = LL_{RIF/GTZC}_TIM2, HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_UART4 = LL_{RIF/GTZC}_UART4, HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_ETH1 = LL_{RIF/GTZC}_{RIMC}_ETH1, ... } hal_{rif/gtzc}_{risc/rimc/tzsc}_periph_t;
Security attributes
typedef enum { HAL_{RIF/GTZC}_NSEC = LL_{RIF/GTZC}_ATTR_NSEC, HAL_{RIF/GTZC}_SEC = LL_{RIF/GTZC}_ATTR_SEC } hal_{rif/gtzc}_sec_attr_t;
Privilege attributes
typedef enum { HAL_{RIF/GTZC}_NPRIV = LL_{RIF/GTZC}_ATTR_NPRIV, HAL_{RIF/GTZC}_PRIV = LL_{RIF/GTZC}_ATTR_PRIV } hal_{rif/gtzc}_priv_attr_t;
Lock status
typedef enum { HAL_{RIF/GTZC}_UNLOCKED = 0U, HAL_{RIF/GTZC}_LOCKED = 1U } hal_{rif/gtzc}_lock_status_t;
Functions:
Security and privilege attribute set/get functions
hal_status_t HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_SetPeriph{AttrName}Attr(hal_{rif/gtzc}_{risc/rimc/tzsc}_periph_t periph, hal_{rif/gtzc}_{attrname}_attr_t attrname_attr); hal_{rif/gtzc}_{attrname}_attr_t HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_GetPeriph{AttrName}Attr(hal_{rif/gtzc}_{risc/rimc/tzsc}_periph_t periph);
Configuration lock functions
hal_status_t HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_Lock{Periph}Config(void / hal_{rif/gtzc}_{risc/rimc/tzsc}_periph_t periph); hal_{rif/gtzc}_lock_status_t HAL_{RIF/GTZC}_{RISC/RIMC/TZSC}_IsLocked{Periph}Config(void / hal_{rif/gtzc}_{risc/rimc/tzsc}_periph_t periph);
Note
Depending on the hardware implementation, the scope of the configuration lock can be:
Applied to the whole block. In this case, the lock functions above do not take parameters (
void), and{Periph}is not included in the function names.Applied with finer granularity to lock the configuration for given peripheral(s). In this case,
{Periph}is included in the function name, and a parameter specifies the peripheral to which the configuration lock applies.
Examples
typedef enum { HAL_RIF_RISC_TIM2 = LL_RIF_TIM2, HAL_RIF_RISC_UART4 = LL_RIF_UART4, ... } hal_rif_risc_periph_t; typedef enum { HAL_RIF_NSEC = LL_RIF_ATTR_NSEC, HAL_RIF_SEC = LL_RIF_ATTR_SEC } hal_rif_sec_attr_t; typedef enum { HAL_RIF_UNLOCKED = 0U, /*!< RIF configuration unlocked */ HAL_RIF_LOCKED = 1U /*!< RIF configuration locked */ } hal_rif_lock_status_t; hal_status_t HAL_RIF_RISC_SetPeriphSecAttr(hal_rif_risc_periph_t periph, hal_rif_sec_attr_t sec_attr); hal_rif_sec_attr_t HAL_RIF_RISC_GetPeriphSecAttr(hal_rif_risc_periph_t periph); hal_status_t HAL_RIF_RISC_LockPeriphConfig(hal_rif_risc_periph_t periph); hal_rif_lock_status_t HAL_RIF_RISC_IsLockedPeriphConfig(hal_rif_risc_periph_t periph); hal_status_t HAL_RIF_RIMC_LockConfig(void); hal_status_t HAL_RIF_RISC_LockConfig(void); hal_rif_lock_status_t HAL_RIF_RIMC_IsLockedConfig(void); hal_rif_lock_status_t HAL_RIF_RISC_IsLockedConfig(void);
typedef enum { HAL_GTZC_TZSC_TIM2 = LL_GTZC_TIM2, HAL_GTZC_TZSC_UART4 = LL_GTZC_UART4, ... } hal_gtzc_tzsc_periph_t; typedef enum { HAL_GTZC_NSEC = LL_GTZC_ATTR_NSEC, HAL_GTZC_SEC = LL_GTZC_ATTR_SEC } hal_gtzc_sec_attr_t; typedef enum { HAL_GTZC_UNLOCKED = 0x00U, /*!< GTZC configuration unlocked */ HAL_GTZC_LOCKED = 0x01U /*!< GTZC configuration locked */ } hal_gtzc_lock_status_t; hal_status_t HAL_GTZC_TZSC_SetPeriphSecAttr(hal_gtzc_tzsc_periph_t periph, hal_gtzc_sec_attr_t sec_attr); hal_gtzc_sec_attr_t HAL_GTZC_TZSC_GetPeriphSecAttr(hal_gtzc_tzsc_periph_t periph); hal_status_t HAL_GTZC_TZSC_LockConfig(void); hal_gtzc_lock_status_t HAL_GTZC_IsLockedConfig(void);
Security and privilege attribute APIs for securable peripherals (RIF_RIFSC/GTZC_TZSC) ¶
Enumerations
Block-based memories
typedef enum { HAL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM1/SRAM1} = LL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM1/SRAM1}, HAL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM2/SRAM2} = LL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM2/SRAM2}, HAL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM3/SRAM3} = LL_{RIF/GTZC}_{RISAB/MPCBB}_{AXISRAM3/SRAM3}, ... } hal_{rif/gtzc}_{risab/mpcbb}_memory_t;
Secure-to-non-secure read/write access status
typedef enum { HAL_{RIF/GTZC}_{RISAB/MPCBB}_SEC_TO_NSEC_DISABLED = 0x00U, HAL_{RIF/GTZC}_{RISAB/MPCBB}_SEC_TO_NSEC_ENABLED = 0x01U } hal_{rif/gtzc}_{risab/mpcbb}_sec_to_nsec_access_status_t;
Memory clock security state (feature available on GTZC only)
typedef enum { HAL_GTZC_MPCBB_CLK_SEC_NOT_INVERTED = LL_GTZC_MPCBB_CLK_SEC_NOT_INVERTED, /*!< GTZC clock security not inverted */ HAL_GTZC_MPCBB_CLK_SEC_INVERTED = LL_GTZC_MPCBB_CLK_SEC_INVERTED /*!< GTZC clock security inverted */ } hal_gtzc_mpcbb_clk_sec_state_t;
Read/write access status (feature available on RIF peripheral only)
typedef enum { HAL_RIF_{READ/WRITE}_DISABLED = LL_RIF_{READ/WRITE}_DISABLED, HAL_RIF_{READ/WRITE}_ENABLED = LL_RIF_{READ/WRITE}_ENABLED } hal_rif_{read/write}_access_status_t;
RIF illegal access status (feature available on RIF peripheral only)
typedef enum { HAL_RIF_ILAC_INACTIVE = 0x00U, HAL_RIF_ILAC_ACTIVE = 0x01U } hal_rif_ilac_status_t;
Note
This enumeration is used to report the illegal access status for both
RIF_RISABandRISAF.RIF illegal access read/write access
typedef enum { HAL_RIF_ILAC_READ = 0x00U, HAL_RIF_ILAC_WRITE = 0x01U } hal_rif_ilac_access_t;
Structure
RIF illegal access memory information structure (not applicable for GTZC)
typedef struct { hal_rif_ilac_access_t access; uint32_t addr; hal_rif_sec_attr_t sec; hal_rif_priv_attr_t priv; } hal_rif_ilac_memory_info_t;
Note
The same structure is used for both
RIF_RISABandRIF_RISAFto provide illegal access information for a block-based memory or for the configuration of a watermark memory.
Functions
Security and privilege attributes Set/Get functions
hal_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_Set{AttrName}Attr{ByBlock/ByAddr}(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory, uint32_t {start_block/offset_byte}, uint32_t {block_nbr/size_byte}, hal_{rif/gtzc}_{attrname}_attr_t attrname_attr); hal_{rif/gtzc}_{attrname}_attr_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_Get{AttrName}Attr{ByBlock/ByAddr}(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory, uint32_t {block/offset_byte});
Note
The same
hal_{rif/gtzc}_{attrname}_attr_tattribute enumeration described in the section Security and privilege attribute APIs for securable peripherals is used.Enabling and disabling secure to non-secure read/write access
hal_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_EnableSecToNSecRdWrAccess(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory); hal_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_DisableSecToNSecRdWrAccess(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory); hal_{rif/gtzc}_{risab/mpcbb}_sec_to_nsec_access_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_IsEnabledSecToNSecRdWrAccess(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory);
Set/Get block based memory clock security state (feature available on GTZC only)
hal_status_t HAL_GTZC_MPCBB_SetClkSecStateInvertion(hal_gtzc_mpcbb_memory_t memory_id, hal_gtzc_mpcbb_clk_sec_state_t clk_sec_state); hal_gtzc_mpcbb_clk_sec_state_t HAL_GTZC_MPCBB_GetClkSecStateInvertion(hal_gtzc_mpcbb_memory_t memory);
Configuration lock
hal_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_LockConfig{ByPage/BySuperBlock/ByAddr}(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory, uint32_t {start_page/start_super_blk/offset_byte}, uint32_t {page_nbr/super_blk_nbr/size_byte}); hal_{rif/gtzc}_lock_status_t HAL_{RIF/GTZC}_{RISAB/MPCBB}_IsLockedConfig{ByPage/BySuperBlock/ByAddr}(hal_{rif/gtzc}_{risab/mpcbb}_memory_t memory, uint32_t {page/super_blk/offset_byte});
Note
The same
hal_{rif/gtzc}_lock_status_tlock status enumeration described in the section Security and privilege attribute APIs for securable peripherals is used.Enable and disable read/write access (feature available on RIF peripheral only)
hal_status_t HAL_RIF_RISAB_{Enable/Disable}{Rd/Wr}Access{ByPage/ByAddr}(hal_rif_risab_memory_t memory, uint32_t {start_page/offset_byte}, uint32_t {page_nbr/size_byte}); hal_rif_{read/write}_access_status_t HAL_RIF_RISAB_IsEnabled{Page/Addr}{Rd/Wr}Access(hal_rif_risab_memory_t memory, uint32_t {page/offset_byte});
Get illegal access info (feature available on RIF peripheral only)
hal_rif_ilac_status_t HAL_RIF_RISAB_IsIllegalConfigAccess(hal_rif_risab_memory_t memory); hal_rif_ilac_status_t HAL_RIF_RISAB_IsIllegalMemoryAccess(hal_rif_risab_memory_t memory); void HAL_RIF_RISAB_GetIllegalMemoryAccessInfo(hal_rif_risab_memory_t memory, hal_rif_ilac_memory_info_t *p_info);
Examples
typedef enum { HAL_RIF_RISAB_AXISRAM1 = LL_RIF_RISAB_AXISRAM1, HAL_RIF_RISAB_AXISRAM2 = LL_RIF_RISAB_AXISRAM2, ... } hal_rif_risab_memory_t; typedef enum { HAL_RIF_RISAB_SEC_TO_NSEC_DISABLED = 0x00U, /*!< RIF RISAB secure read/write data accesses to non-secure blocks and pages disabled */ HAL_RIF_RISAB_SEC_TO_NSEC_ENABLED = 0x01U /*!< RIF RISAB secure read/write data accesses to non-secure blocks and pages enabled */ } hal_rif_risab_sec_to_nsec_access_status_t;
hal_status_t HAL_RIF_RISAB_SetSecAttrByBlock(hal_rif_risab_memory_t memory, uint32_t start_block, uint32_t block_nbr, hal_rif_sec_attr_t sec_attr); hal_status_t HAL_RIF_RISAB_SetPrivAttrByBlock(hal_rif_risab_memory_t memory, uint32_t start_block, uint32_t block_nbr, hal_rif_priv_attr_t priv_attr); hal_rif_sec_attr_t HAL_RIF_RISAB_GetSecAttrByBlock(hal_rif_risab_memory_t memory, uint32_t block); hal_rif_priv_attr_t HAL_RIF_RISAB_GetPrivAttrByBlock(hal_rif_risab_memory_t memory, uint32_t block); hal_status_t HAL_RIF_RISAB_EnableSecToNSecRdWrAccess(hal_rif_risab_memory_t memory); hal_status_t HAL_RIF_RISAB_DisableSecToNSecRdWrAccess(hal_rif_risab_memory_t memory); hal_rif_risab_sec_to_nsec_access_status_t HAL_RIF_RISAB_IsEnabledSecToNSecRdWrAccess(hal_rif_risab_memory_t memory); hal_status_t HAL_RIF_RISAB_SetSecAttrByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte, hal_rif_sec_attr_t sec_attr); hal_status_t HAL_RIF_RISAB_SetPrivAttrByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte, hal_rif_priv_attr_t priv_attr); hal_rif_sec_attr_t HAL_RIF_RISAB_GetSecAttrByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte); hal_rif_priv_attr_t HAL_RIF_RISAB_GetPrivAttrByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte); hal_status_t HAL_RIF_RISAB_EnableRdAccessByPage(hal_rif_risab_memory_t memory, uint32_t start_page, uint32_t page_nbr); hal_status_t HAL_RIF_RISAB_DisableRdAccessByPage(hal_rif_risab_memory_t memory, uint32_t start_page, uint32_t page_nbr); hal_rif_read_access_status_t HAL_RIF_RISAB_IsEnabledPageRdAccess(hal_rif_risab_memory_t memory, uint32_t page); hal_status_t HAL_RIF_RISAB_EnableWrAccessByPage(hal_rif_risab_memory_t memory, uint32_t start_page, uint32_t page_nbr); hal_status_t HAL_RIF_RISAB_DisableWrAccessByPage(hal_rif_risab_memory_t memory, uint32_t start_page, uint32_t page_nbr); hal_rif_write_access_status_t HAL_RIF_RISAB_IsEnabledPageWrAccess(hal_rif_risab_memory_t memory, uint32_t page); hal_status_t HAL_RIF_RISAB_EnableRdAccessByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte); hal_status_t HAL_RIF_RISAB_DisableRdAccessByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte); hal_rif_read_access_status_t HAL_RIF_RISAB_IsEnabledAddrRdAccess(hal_rif_risab_memory_t memory, uint32_t offset_byte); hal_status_t HAL_RIF_RISAB_EnableWrAccessByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte); hal_status_t HAL_RIF_RISAB_DisableWrAccessByAddr(hal_rif_risab_memory_t memory, uint32_t offset_byte, uint32_t size_byte); hal_rif_write_access_status_t HAL_RIF_RISAB_IsEnabledAddrWrAccess(hal_rif_risab_memory_t memory, uint32_t offset_byte);
typedef enum { HAL_GTZC_MPCBB_SRAM1 = (uint32_t)LL_GTZC_MPCBB_SRAM1, /*!< GTZC block based SRAM1 memory */ HAL_GTZC_MPCBB_SRAM2 = (uint32_t)LL_GTZC_MPCBB_SRAM2, /*!< GTZC block based SRAM2 memory */ #if defined(SRAM3_BASE) HAL_GTZC_MPCBB_SRAM3 = (uint32_t)LL_GTZC_MPCBB_SRAM3, /*!< GTZC block based SRAM3 memory */ #endif /* SRAM3_BASE */ HAL_GTZC_MPCBB_SRAM4 = (uint32_t)LL_GTZC_MPCBB_SRAM4, /*!< GTZC block based SRAM4 memory */ #if defined(SRAM5_BASE) HAL_GTZC_MPCBB_SRAM5 = (uint32_t)LL_GTZC_MPCBB_SRAM5, /*!< GTZC block based SRAM5 memory */ #endif /* SRAM5_BASE */ #if defined(SRAM6_BASE) HAL_GTZC_MPCBB_SRAM6 = (uint32_t)LL_GTZC_MPCBB_SRAM6 /*!< GTZC block based SRAM6 memory */ #endif /* SRAM6_BASE */ } hal_gtzc_mpcbb_memory_t; typedef enum { HAL_GTZC_MPCBB_SEC_TO_NSEC_DISABLED = 0x00U, HAL_GTZC_MPCBB_SEC_TO_NSEC_ENABLED = 0x01U } hal_gtzc_mpcbb_sec_to_nsec_access_status_t; typedef enum { HAL_GTZC_MPCBB_CLK_SEC_NOT_INVERTED = LL_GTZC_MPCBB_CLK_SEC_NOT_INVERTED, /*!< GTZC clock security not inverted */ HAL_GTZC_MPCBB_CLK_SEC_INVERTED = LL_GTZC_MPCBB_CLK_SEC_INVERTED /*!< GTZC clock security inverted */ } hal_gtzc_mpcbb_clk_sec_state_t;
hal_status_t HAL_GTZC_MPCBB_SetSecAttrByBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t start_block, uint32_t block_nbr, hal_gtzc_sec_attr_t sec_attr); hal_status_t HAL_GTZC_MPCBB_SetPrivAttrByBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t start_block, uint32_t block_nbr, hal_gtzc_priv_attr_t priv_attr); hal_gtzc_sec_attr_t HAL_GTZC_MPCBB_GetSecAttrByBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t block); hal_gtzc_priv_attr_t HAL_GTZC_MPCBB_GetPrivAttrByBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t block); hal_status_t HAL_GTZC_MPCBB_EnableSecToNSecRdWrAccess(hal_gtzc_mpcbb_memory_t memory); hal_status_t HAL_GTZC_MPCBB_DisableSecToNSecRdWrAccess(hal_gtzc_mpcbb_memory_t memory); hal_gtzc_mpcbb_sec_to_nsec_access_status_t HAL_GTZC_MPCBB_IsEnabledSecToNSecRdWrAccess(hal_gtzc_mpcbb_memory_t memory); hal_status_t HAL_GTZC_MPCBB_SetClkSecStateInvertion(hal_gtzc_mpcbb_memory_t memory_id, hal_gtzc_mpcbb_clk_sec_state_t clk_sec_state); hal_gtzc_mpcbb_clk_sec_state_t HAL_GTZC_MPCBB_GetClkSecStateInvertion(hal_gtzc_mpcbb_memory_t memory); hal_status_t HAL_GTZC_MPCBB_LockConfigBySuperBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t start_super_blk, uint32_t super_blk_nbr); hal_gtzc_lock_status_t HAL_GTZC_MPCBB_IsLockedConfigBySuperBlock(hal_gtzc_mpcbb_memory_t memory, uint32_t super_blk); hal_status_t HAL_GTZC_MPCBB_SetSecAttrByAddr(hal_gtzc_mpcbb_memory_t memory, uint32_t offset_byte, uint32_t size_byte, hal_gtzc_sec_attr_t sec_attr); hal_status_t HAL_GTZC_MPCBB_SetPrivAttrByAddr(hal_gtzc_mpcbb_memory_t memory, uint32_t offset_byte, uint32_t size_byte, hal_gtzc_priv_attr_t priv_attr); hal_gtzc_sec_attr_t HAL_GTZC_MPCBB_GetSecAttrByAddr(hal_gtzc_mpcbb_memory_t memory, uint32_t offset_byte); hal_gtzc_priv_attr_t HAL_GTZC_MPCBB_GetPrivAttrByAddr(hal_gtzc_mpcbb_memory_t memory, uint32_t offset_byte);
Security and privilege attribute APIs for watermark memories (RIF_RISAF/ GTZC_TZSC-MPCWM) ¶
Note
On the
RIF_RISAFperipheral, it is possible to define both regions and subregions. OnGTZC_MPCWM, only subregions can be defined.Enabling and disabling read and write access is possible only on the
RIF_RISAFperipheral and is configured by subregion.Locking the configuration is possible on both
RIF_RISAFandGTZC_MPCWMand is configured by subregion.For generalization, both region-based and subregion-based variants of the APIs below must be provided for RIF. For GTZC, only the subregion-based API variant must be provided, and in this case there is no
regionparameter.
Enumerations
RIF_RISAF/GTZC_TZSC-MPCWM memories
typedef enum { HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{XSPI1/OCTOSPI1} = LL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{XSPI1/OCTOSPI1}, HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{XSPI2/OCTOSPI2} = LL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{XSPI2/OCTOSPI2}, ... } hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t;
RIF_RISAF regions (not applicable for GTZC)
typedef enum { HAL_RIF_RISAF_REGION_1 = LL_RIF_RISAF_REGION_1, /*!< RIF RISAF region 1 */ HAL_RIF_RISAF_REGION_2 = LL_RIF_RISAF_REGION_2, /*!< RIF RISAF region 2 */ ... } hal_rif_risaf_region_t;
RIF_RISAF/GTZC_TZSC-MPCWM subregions
typedef enum { HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_SUBREGION_A = LL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_SUBREGION_A, HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_SUBREGION_B = LL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_SUBREGION_B } hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t;
RIF_RISAF/GTZC_TZSC-MPCWM Region and subregion enabled status
typedef enum { HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{REGION/SUBREGION}_DISABLED = 0U, HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{REGION/SUBREGION}_ENABLED = 1U } hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_{region/subregion}_status_t;
Functions
Defining the region or the subregion: Set/get boundaries
hal_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_Set{Region/SubRegion}Boundaries(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, /* applicable for RIF only */ hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion, uint32_t offset_byte, uint32_t size_byte); void HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_Get{Region/SubRegion}Boundaries(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, /* applicable for RIF only */ hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion, uint32_t *offset_byte, uint32_t *size_byte);
Note
For the RIF-RISAF peripheral, it is possible to define regions and subregions. On the GTZC-MPCWM, it is possible to define subregions only. Thus:
For RIF, both region and subregion variants of the APIs must be provided.
For GTZC, only the subregion variant of the API must be provided. In this GTZC case, there is no ‘region’ parameter (see also the next examples for RIF and GTZC).
Set/get attributes for a region/subregion
hal_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_Set{Region/SubRegion}{AttrName}Attr(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, /* applicable for RIF only */ hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion, hal_{rif/gtzc}_{attrname}_attr_t attrname_attr); hal_{rif/gtzc}_{attrname}_attr_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_Get{Region/SubRegion}{AttrName}Attr(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, /* applicable for RIF only */ hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion);
Enable and disable read/write access for a subregion
Note
Enabling and disabling read and write access is possible only on the
RIF_RISAFperipheral and is configured by subregion. This feature is not available onGTZC_MPCWM.The same
hal_rif_{read/write}_access_status_tenumeration used forRIF_RISABis also used forRIF_RISAFto specify the read/write access status.hal_status_t HAL_RIF_RISAF_{Enable/Disable}SubRegion{Rd/Wr}Access(hal_rif_risaf_memory_t memory, hal_rif_risaf_region_t region, hal_rif_risaf_subregion_t subregion); hal_rif_{read/write}_access_status_t HAL_RIF_RISAF_IsEnabledSubRegion{Rd/Wr}Access(hal_rif_risaf_memory_t memory, hal_rif_risaf_region_t region, hal_rif_risaf_subregion_t subregion);
Enable and disable a region/subregion
Note
As described above, RIF supports both region-level and subregion-level configuration, so both API levels must be provided. GTZC supports only subregion-level configuration; therefore, only subregion APIs must be provided.
hal_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_{Enable/Disable}{Region/SubRegion}(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion); hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_{region/subregion}_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_IsEnabled{Region/SubRegion}(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion);
Lock a subregion configuration
Note
Configuration locking is supported on both RIF-RISAF and GTZC-MPCWM, and can be applied independently to each subregion.
hal_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_LockSubRegionConfig(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion); hal_{rif/gtzc}_lock_status_t HAL_{RIF/GTZC}_{RISAF/TZSC_MPCWM}_IsLockedSubRegionConfig(hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_memory_t memory, hal_rif_risaf_region_t region, hal_{rif/gtzc}_{risaf/tzsc_mpcwm}_subregion_t subregion);
Note
The same
hal_{rif/gtzc}_lock_status_tlock status enumeration described in the section Security and privilege attribute APIs for securable peripherals is used to describe the lock status.RIF_RISAF, illegal access, status and information functions (not possible on GTZC)
hal_rif_ilac_status_t HAL_RIF_RISAF_IsIllegalConfigAccess(hal_rif_risaf_memory_t memory); hal_rif_ilac_status_t HAL_RIF_RISAF_IsIllegalMemoryAccess(hal_rif_risaf_memory_t memory); void HAL_RIF_RISAF_GetIllegalMemoryAccessInfo(hal_rif_risaf_memory_t memory, hal_rif_ilac_memory_info_t *p_info);
Note
The same
hal_rif_ilac_status_t
enumeration and
hal_rif_ilac_memory_info_t
structure described in the section
Security and privilege attribute APIs for block-based memories (RIF_RISAB / GTZC_MPCBB)
are used for both
RIF_RISAB
and
RIF_RISAF.
Examples
typedef enum
{
HAL_RIF_RISAF_XSPI1 = LL_RIF_RISAF_XSPI1,
HAL_RIF_RISAF_XSPI2 = LL_RIF_RISAF_XSPI2,
HAL_RIF_RISAF_FMC = LL_RIF_RISAF_FMC,
HAL_RIF_RISAF_BKPRAM = LL_RIF_RISAF_BKPRAM
} hal_rif_risaf_memory_t;
typedef enum
{
HAL_RIF_RISAF_REGION_1 = LL_RIF_RISAF_REGION_1,
..,
HAL_RIF_RISAF_REGION_7 = LL_RIF_RISAF_REGION_7
} hal_rif_risaf_region_t;
typedef enum
{
HAL_RIF_RISAF_SUBREGION_A = LL_RIF_RISAF_SUBREGION_A,
HAL_RIF_RISAF_SUBREGION_B = LL_RIF_RISAF_SUBREGION_B
} hal_rif_risaf_subregion_t;
typedef enum
{
HAL_RIF_RISAF_REGION_DISABLED = 0x00U,
HAL_RIF_RISAF_REGION_ENABLED = 0x01U
} hal_rif_risaf_region_status_t;
typedef enum
{
HAL_RIF_RISAF_SUBREGION_DISABLED = 0x00U,
HAL_RIF_RISAF_SUBREGION_ENABLED = 0x01U
} hal_rif_risaf_subregion_status_t;
hal_status_t HAL_RIF_RISAF_SetRegionBoundaries(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
uint32_t offset_byte,
uint32_t size_byte);
void HAL_RIF_RISAF_GetRegionBoundaries(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
uint32_t *offset_byte,
uint32_t *size_byte);
hal_status_t HAL_RIF_RISAF_SetSubRegionBoundaries(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion,
uint32_t offset_byte,
uint32_t size_byte);
void HAL_RIF_RISAF_GetSubRegionBoundaries(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion,
uint32_t *offset_byte,
uint32_t *size_byte);
hal_status_t HAL_RIF_RISAF_SetRegionSecAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_sec_attr_t sec_attr);
hal_status_t HAL_RIF_RISAF_SetRegionPrivAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_priv_attr_t priv_attr);
hal_rif_sec_attr_t HAL_RIF_RISAF_GetRegionSecAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region);
hal_rif_priv_attr_t HAL_RIF_RISAF_GetRegionPrivAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region);
hal_status_t HAL_RIF_RISAF_SetSubRegionSecAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion,
hal_rif_sec_attr_t sec_attr);
hal_status_t HAL_RIF_RISAF_SetSubRegionPrivAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion,
hal_rif_priv_attr_t priv_attr);
hal_rif_sec_attr_t HAL_RIF_RISAF_GetSubRegionSecAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_priv_attr_t HAL_RIF_RISAF_GetSubRegionPrivAttr(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_EnableSubRegionWrAccess(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_DisableSubRegionWrAccess(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_EnableSubRegionRdAccess(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_DisableSubRegionRdAccess(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_write_access_status_t HAL_RIF_RISAF_IsEnabledWrAccessSubRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_read_access_status_t HAL_RIF_RISAF_IsEnabledRdAccessSubRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_EnableRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region);
hal_status_t HAL_RIF_RISAF_DisableRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region);
hal_rif_risaf_region_status_t HAL_RIF_RISAF_IsEnabledRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region);
hal_status_t HAL_RIF_RISAF_EnableSubRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_DisableSubRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_risaf_subregion_status_t HAL_RIF_RISAF_IsEnabledSubRegion(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_status_t HAL_RIF_RISAF_LockSubRegionConfig(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_lock_status_t HAL_RIF_RISAF_IsLockedSubRegionConfig(hal_rif_risaf_memory_t memory,
hal_rif_risaf_region_t region,
hal_rif_risaf_subregion_t subregion);
hal_rif_ilac_status_t HAL_RIF_RISAF_IsIllegalConfigAccess(hal_rif_risaf_memory_t memory);
hal_rif_ilac_status_t HAL_RIF_RISAF_IsIllegalMemoryAccess(hal_rif_risaf_memory_t memory);
void HAL_RIF_RISAF_GetIllegalMemoryAccessInfo(hal_rif_risaf_memory_t memory,
hal_rif_ilac_memory_info_t *p_info);
typedef enum
{
HAL_GTZC_TZSC_MPCWM_XSPI1 = LL_GTZC_TZSC_MPCWM_XSPI1,
HAL_GTZC_TZSC_MPCWM_XSPI2 = LL_GTZC_TZSC_MPCWM_XSPI2,
...
} hal_gtzc_tzsc_mpcwm_memory_t;
typedef enum
{
HAL_GTZC_TZSC_MPCWM_SUBREGION_A = LL_GTZC_TZSC_MPCWM_SUBREGION_A,
HAL_GTZC_TZSC_MPCWM_SUBREGION_B = LL_GTZC_TZSC_MPCWM_SUBREGION_B
} hal_gtzc_tzsc_mpcwm_subregion_t;
typedef enum
{
HAL_GTZC_TZSC_MPCWM_SUBREGION_DISABLED = 0x00U,
HAL_GTZC_TZSC_MPCWM_SUBREGION_ENABLED = 0x01U
} hal_gtzc_tzsc_mpcwm_subregion_status_t;
hal_status_t HAL_GTZC_TZSC_MPCWM_SetSubRegionBoundaries(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion,
uint32_t offset_byte,
uint32_t size_byte);
void HAL_GTZC_TZSC_MPCWM_GetSubRegionBoundaries(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion,
uint32_t *offset_byte,
uint32_t *size_byte);
hal_status_t HAL_GTZC_TZSC_MPCWM_SetSubRegionSecAttr(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion,
hal_gtzc_sec_attr_t sec_attr);
hal_gtzc_sec_attr_t HAL_GTZC_TZSC_MPCWM_GetSubRegionSecAttr(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion);
hal_status_t HAL_GTZC_TZSC_MPCWM_SetSubRegionPrivAttr(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion,
hal_gtzc_priv_attr_t priv_attr);
hal_gtzc_priv_attr_t HAL_GTZC_TZSC_MPCWM_GetSubRegionPrivAttr(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion);
hal_status_t HAL_GTZC_TZSC_MPCWM_EnableSubRegion(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion);
hal_status_t HAL_GTZC_TZSC_MPCWM_DisableSubRegion(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion);
hal_gtzc_tzsc_mpcwm_subregion_status_t HAL_GTZC_TZSC_MPCWM_IsEnabledSubRegion(hal_gtzc_tzsc_mpcwm_memory_t memory,
hal_gtzc_tzsc_mpcwm_subregion_t subregion);
Illegal access ¶
The illegal access detection feature applies upon any security illegal access: i.e for RIF/GTZC aware peripherals, securable peripherals, Block based and watermark.
Enumerations
Illegal access peripherals
typedef enum { HAL_{RIF/GTZC}_{IAC/TZIC}_TIM2 = LL_{RIF/GTZC}_TIM2, HAL_{RIF/GTZC}_{IAC/TZIC}_UART4 = LL_{RIF/GTZC}_UART4, HAL_{RIF/GTZC}_{IAC/TZIC}_ETH1 = LL_{RIF/GTZC}_{RIMC}_ETH1, ... } hal_{rif/gtzc}_{iac/tzic}_periph_t;
Illegal access interrupt status
typedef enum { HAL_{RIF/GTZC}_{IAC/TZIC}_IT_DISABLED = 0U, HAL_{RIF/GTZC}_{IAC/TZIC}_IT_ENABLED = 1U } hal_{rif/gtzc}_{iac/tzic}_it_status_t;
Functions
Illegal access interrupt management functions (enable/disable, IRQ handler, and callback)
void HAL_{RIF/GTZC}_{IAC/TZIC}_EnableIT(hal_{rif/gtzc}_{iac/tzic}_periph_t periph); void HAL_{RIF/GTZC}_{IAC/TZIC}_DisableIT(hal_{rif/gtzc}_{iac/tzic}_periph_t periph); hal_{rif/gtzc}_{iac/tzic}_it_status_t HAL_{RIF/GTZC}_{IAC/TZIC}_IsEnabledIT(hal_{rif/gtzc}_{iac/tzic}_periph_t periph); void HAL_{RIF/GTZC}_{IAC/TZIC}_IRQHandler(void); void HAL_{RIF/GTZC}_{IAC/TZIC}_Callback(hal_{rif/gtzc}_{iac/tzic}_periph_t periph);
Examples
typedef enum
{
HAL_RIF_IAC_TIM2 = LL_RIF_TIM2,
...
} hal_rif_iac_periph_t;
typedef enum
{
HAL_RIF_IAC_IT_DISABLED = 0U,
HAL_RIF_IAC_IT_ENABLED = 1U
} hal_rif_iac_it_status_t;
hal_status_t HAL_RIF_IAC_EnableIT(hal_rif_iac_periph_t periph);
hal_status_t HAL_RIF_IAC_DisableIT(hal_rif_iac_periph_t periph);
hal_rif_iac_it_status_t HAL_RIF_IAC_IsEnabledIT(hal_rif_iac_periph_t periph);
void HAL_RIF_IAC_IRQHandler(void);
void HAL_RIF_IAC_Callback(hal_rif_iac_periph_t periph);
typedef enum
{
HAL_GTZC_TZIC_TIM2 = LL_GTZC_TIM2,
...
} hal_gtzc_tzic_periph_t;
typedef enum
{
HAL_GTZC_TZIC_IT_DISABLED = 0U,
HAL_GTZC_TZIC_IT_ENABLED = 1U
} hal_gtzc_tzic_it_status_t;
hal_status_t HAL_GTZC_TZIC_EnableIT(hal_gtzc_tzic_periph_t periph);
hal_status_t HAL_GTZC_TZIC_DisableIT(hal_gtzc_tzic_periph_t periph);
hal_gtzc_tzic_it_status_t HAL_GTZC_TZIC_IsEnabledIT(hal_gtzc_tzic_periph_t periph);
void HAL_GTZC_TZIC_IRQHandler(void);
void HAL_GTZC_TZIC_Callback(hal_gtzc_tzic_periph_t periph);
HAL and LL RIF-aware/TZ-aware peripherals APIs ¶
The HAL and LL layers must include TrustZone (TZ)-aware and RIF-aware PPP attribute management functions, with each TZ-aware/RIF-aware PPP HAL and LL module providing its own attribute management APIs. Attribute management must be provided as a standalone capability. The RIF-aware/TZ-aware HAL PPP attribute APIs must be callable independently of the HAL PPP handle initialization, with the HAL PPP instance as the first parameter replacing the traditional handle parameter. See also paragraph HAL PPP instance retrieving to understand how to get the PPP peripheral instance from the HAL PPP handle.
Attribute functions must be unified across TZ-aware modules and families, and when possible, between RIF and TZ implementations.
Items (such as PVD and WKUPPIN) must be clearly separated from their attributes (Secure/NSecure).
Except for the attribute-setting functions, no other HAL or LL function within any module must impact the configured TZ/RIF attributes, ensuring system integrity. Function usage must support both static configurations aligned with Trusted Execution Environment requirements (also called isolation) and dynamic reconfiguration to adjust attributes according to application needs.
In the application code, when the RIF-aware/TZ-aware HAL/LL PPP attribute functions are called statically (i.e. from the isolation part), it must directly use the required instance.
// Using LL driver
LL_PPP_Func(PPPn, ...);
// Using HAL driver
HAL_PPP_Func(HAL_PPPn, ...);
When these functions are called dynamically (to reconfigure/adjust the attributes according to the application needs), the application must use the appropriate function to retrieve the instance from the handle (if the given driver uses a handle) and use it to call the attribute function.
// Using LL driver
LL_PPP_Func(HAL_PPP_GetLLInstance(hppp), ...);
// Using HAL driver
HAL_PPP_Func(HAL_PPP_GetInstance(hppp), ...);
LL RIF-aware/TZ-aware peripherals APIs ¶
Attribute management functions
__STATIC_INLINE void LL_{PPP}_{SUBBLOCK}_Set{AttrName}Attr({PPP_TypeDef *pppx}, {uint32_t item/subinstance}, uint32_t {attrname}_attr); __STATIC_INLINE uint32_t LL_{PPP}_{SUBBLOCK}_Get{AttrName}Attr({PPP_TypeDef *pppx}, {uint32_t item/subinstance}); __STATIC_INLINE void LL_{PPP}_{SUBBLOCK}_Lock{AttrName}Attr({PPP_TypeDef *pppx}, {uint32_t items/subinstances}); __STATIC_INLINE void LL_{PPP}_{SUBBLOCK}_Unlock{AttrName}Attr({PPP_TypeDef *pppx}, {uint32_t items/subinstances}); __STATIC_INLINE uint32_t LL_{PPP}_{SUBBLOCK}_IsLocked{AttrName}Attr({PPP_TypeDef *pppx}, {uint32_t item/subinstance});
With:
The
{PPP}is the name of the peripheral.The
{SUBBLOCK}(when existing) within a TZ-aware/RIF-aware LL module must be applied to the set/get attribute APIs.The
{AttrName}is the attribute abbreviation described here: -Sec,Priv,Public
pppx
is:
- The physical instance of type
PPP_TypeDef*
when existing in the given driver (e.g. LL FLASH).
Omitted when the given HAL driver does not use an instance, like the LL RCC or PWR.
Items/subinstances:
Use subinstances when the attribute applies to sub‑instances meaning multiple identical resources of the same peripherals (e.g. pins in case of the GPIO). In this case these APIs reuse the already existing subinstances naming and definitions (e.g. in case of GPIO, subinstances = pins and must be set to the defines
LL_GPIO_PIN_n).Use items when the attribute applies to heterogeneous/specific parts of the given peripheral instance (e.g. the RCC oscillators and PLLs and other items). In this case a set of dedicated defines is provided to list these items with the following naming rules
LL_{PPP}_{ATTRNAME}_ITEM_{ITEM},LL_{PPP}_{ATTRNAME}_ITEM_ALLbeing required.Omitted when the attributes setting or lock apply to the given PPP instance. In this case only the
pppxinstance is used if the LL driver already uses it, if not the function becomesvoid.
Note
Set attributes APIs can be applied for one or several items/subinstances (defines can be ORed/combined when possible).
Get attributes APIs must be applied for one single item/subinstance (cannot be ORed/combined).
Lock/Unlock/IsLocked APIs parameters (instance, items/subinstances) must be aligned with:
the given LL driver: whether it uses a
PPP_TypeDefinstance or not (case of the RCC),the given device capability (whether the lock can be performed at instance granularity or at item/sub‑instance granularity).
The unlock function must be provided only if it is possible to unlock on the fly (i.e. without the need of a system reset).
The
IsLockedAPI must return the numerical value1when locked and0when unlocked (same as all otherLL_PPP_IsxxxAPIs).
Examples
RCC
#define LL_RCC_ATTR_NSEC 0UL #define LL_RCC_ATTR_SEC 1UL #define LL_RCC_ATTR_NPRIV 0UL #define LL_RCC_ATTR_PRIV 1UL #define LL_RCC_ATTR_NPUBLIC 0UL #define LL_RCC_ATTR_PUBLIC 1UL #define LL_RCC_SEC_ITEM_HSE RCC_SECCFGR_HSE ... #define LL_RCC_SEC_ITEM_PERIPHCLK RCC_SECCFGR_PER #define LL_RCC_SEC_ITEM_ALL RCC_SECURE_MASK #define LL_RCC_PRIV_ITEM_SYSCLK RCC_PRIVCFGR_SYS ... #define LL_RCC_PRIV_ITEM_PERIPHCLK RCC_PRIVFGR_PERIPH #define LL_RCC_PRIV_ITEM_ALL RCC_PRIVRE_MASK #define LL_RCC_LOCK_ITEM_RESET_FLAGS RCC_RCFGLOCKR_RMVF ... #define LL_RCC_LOCK_ITEM_PERIPHCLK RCC_RCFGLOCKR_PERIPH #define LL_RCC_LOCK_ITEM_ALL RCC_PRIVRE_MASK
__STATIC_INLINE void LL_RCC_SetSecAttr(uint32_t item, uint32_t sec_attr); __STATIC_INLINE uint32_t LL_RCC_GetSecAttr(uint32_t item); __STATIC_INLINE void LL_RCC_SetPrivAttr(uint32_t item, uint32_t priv_attr); __STATIC_INLINE uint32_t LL_RCC_GetPrivAttr(uint32_t item); __STATIC_INLINE void LL_RCC_LockAttr(uint32_t item); __STATIC_INLINE uint32_t LL_RCC_IsLockedAttr(uint32_t item);
Note
In this LL RCC example:
The instance is omitted as it is not used in the LL RCC driver.
Items are used, as the attribute setting applies to heterogeneous (non-identical) parts of the RCC such as HSE, LSE, etc.
Locking is possible per item in this example.
No unlock API is provided, as unlock is not possible (unlock is performed by a system reset).
GPIO
#define LL_GPIO_PIN_0 GPIO_BSRR_BS0 /*!< Select pin 0 */
#define LL_GPIO_PIN_1 GPIO_BSRR_BS1 /*!< Select pin 1 */
...
#define LL_GPIO_PIN_14 GPIO_BSRR_BS14 /*!< Select pin 14 */
#define LL_GPIO_PIN_15 GPIO_BSRR_BS15 /*!< Select pin 15 */
#define LL_GPIO_PIN_ALL
#define LL_GPIO_ATTR_NSEC 0U /*!< I/O pin is non-secure */
#define LL_GPIO_ATTR_SEC GPIO_SECCFGR_SEC0 /*!< I/O pin is secure */
#define LL_GPIO_ATTR_NPRIV 0U /*!< I/O pin is unprivileged */
#define LL_GPIO_ATTR_PRIV GPIO_PRIVCFGR_PRIV0 /*!< I/O pin is privileged */
__STATIC_INLINE void LL_GPIO_SetSecAttr(GPIO_TypeDef *gpiox,
uint32_t pin_mask,
uint32_t sec_attr);
__STATIC_INLINE uint32_t LL_GPIO_GetSecAttr(const GPIO_TypeDef *gpiox,
uint32_t pin);
__STATIC_INLINE void LL_GPIO_SetPrivAttr(GPIO_TypeDef *gpiox,
uint32_t pin_mask,
uint32_t priv_attr);
__STATIC_INLINE uint32_t LL_GPIO_GetPrivAttr(const GPIO_TypeDef *gpiox,
uint32_t pin);
__STATIC_INLINE void LL_GPIO_LockAttr(GPIO_TypeDef *gpiox, uint32_t pin_mask);
__STATIC_INLINE uint32_t LL_GPIO_IsLockedAttr(const GPIO_TypeDef *gpiox, uint32_t pin);
Note
In this LL GPIO example:
The
GPIO_TypeDefinstance is used and corresponds to the GPIO port.The subinstances are the pins, using the same
LL_GPIO_PIN_ndefines as the overall driver.The attributes lock can be done by pin(s) in the above example.
The attributes IsLocked API return the numerical values “0” or “1”.
EXTI
#define LL_EXTI_LINE_0 EXTI_IMR1_IM0 /*!< Extended line 0 */
...
#define LL_EXTI_LINE_31 EXTI_IMR1_IM31 /*!< Extended line 31 */
#define LL_EXTI_LINE_ALL_0_31 EXTI_IMR1_IM_ALL /*!< All extended lines from 0 to 31 */
#define LL_EXTI_LINE_32 EXTI_IMR2_IM32 /*!< Extended line 32 */
...
#define LL_EXTI_LINE_63 EXTI_IMR2_IM63 /*!< Extended line 63 */
#define LL_EXTI_LINE_ALL_32_63 EXTI_IMR2_IM_ALL /*!< All extended lines from 32 to 63 */
#define LL_EXTI_ATTR_NSEC 0U
#define LL_EXTI_ATTR_SEC 1U
#define LL_EXTI_ATTR_NPRIV 0U
#define LL_EXTI_ATTR_PRIV 1U
/**
* @param exti_line This parameter can be a combination of the following values:
* @arg @ref LL_EXTI_LINE_0
* @arg @ref LL_EXTI_LINE_1
* ...
* @arg @ref LL_EXTI_LINE_31
*/
__STATIC_INLINE void LL_EXTI_SetSecAttr_0_31(uint32_t exti_line, uint32_t sec_attr);
/**
* @param exti_line This parameter can be one of the following values:
* @arg @ref LL_EXTI_LINE_0
* @arg @ref LL_EXTI_LINE_1
* ...
* @arg @ref LL_EXTI_LINE_31
*/
__STATIC_INLINE uint32_t LL_EXTI_GetSecAttr_0_31(uint32_t exti_line);
/**
* @param exti_line This parameter can be a combination of the following values:
* @arg @ref LL_EXTI_LINE_32
* @arg @ref LL_EXTI_LINE_33
* ...
* @arg @ref LL_EXTI_LINE_63
*/
__STATIC_INLINE void LL_EXTI_SetSecAttr_32_63(uint32_t exti_line, uint32_t sec_attr);
/**
* @param exti_line This parameter can be one of the following values:
* @arg @ref LL_EXTI_LINE_32
* @arg @ref LL_EXTI_LINE_33
* ...
* @arg @ref LL_EXTI_LINE_63
*/
__STATIC_INLINE uint32_t LL_EXTI_GetSecAttr_32_63(uint32_t exti_line);
/* Same pattern for SetPrivAttr/GetPrivAttr APIs */
__STATIC_INLINE void LL_EXTI_LockAttr(void);
__STATIC_INLINE uint32_t LL_EXTI_IsLockedAttr(void); /* Returns numerical values 0 or 1 */
Note
In this LL EXTI example:
The instance is omitted, as the LL EXTI driver does not use an
EXTI_TypeDefinstance.The subinstances are the EXTI lines, using the same
LL_EXTI_LINE_ndefines as the rest of the LL EXTI driver.The line defines can be combined (ORed) for the
SetAPIs, but not for theGetAPIs.The
LockAttrandIsLockedAttrfunctions take no parameter in this example, as the hardware allows locking all line attributes together.The
IsLockedAttrAPI returns the numerical values0or1.
NVM
#define LL_NVM_ATTR_NSEC 0UL
#define LL_NVM_ATTR_SEC 1UL
#define LL_NVM_ATTR_NPRIV 0UL
#define LL_NVM_ATTR_PRIV 1UL
#define LL_NVM_SEC_ITEM_PM NVM_SECCFGR_PM
#define LL_NVM_SEC_ITEM_PERF NVM_SECCFGR_PERF
..
#define LL_NVM_SEC_ITEM_ALL ..
#define LL_NVM_PRIV_ITEM_PM NVM_PRIVCFGR_PM
..
#define LL_NVM_PRIV_ITEM_ALL ..
#define LL_NVM_LOCK_ITEM_PM NVM_RCFGLOCKR_PM
..
#define LL_NVM_LOCK_ITEM_ALL ..
__STATIC_INLINE void LL_NVM_SetSecAttr(NVM_TypeDef *nvmx,
uint32_t item,
uint32_t sec_attr);
__STATIC_INLINE uint32_t LL_NVM_GetSecAttr(const NVM_TypeDef *nvmx,
uint32_t item);
__STATIC_INLINE void LL_NVM_SetPrivAttr(NVM_TypeDef *nvmx,
uint32_t item,
uint32_t priv_attr);
__STATIC_INLINE uint32_t LL_NVM_GetPrivAttr(const NVM_TypeDef *nvmx,
uint32_t item);
__STATIC_INLINE void LL_NVM_LockAttr(NVM_TypeDef *nvmx,
uint32_t item);
__STATIC_INLINE uint32_t LL_NVM_IsLockedAttr(const NVM_TypeDef *nvmx,
uint32_t item);
Note
In this LL NVM example, the attributes APIs use:
The existing instance of type
NVM_TypeDefitems as the attributes setting applies to heterogenous parts (not identical) of the NVM. The items can be combined for the
SetandLockAPIs. Not for theGet/IsLockedAPIs.The IsLocked API returns the numeric values
0or1.
DMA
#define LL_DMA_CHANNEL_0 0x01UL
#define LL_DMA_CHANNEL_1 0x02UL
...
#define LL_DMA_CHANNEL_15 0x8000UL
#define LL_DMA_CHANNEL_ALL 0xFFFFUL
/* Channel security items */
#define LL_DMA_SEC_ITEM_SRC DMA_CTR1_SSEC
#define LL_DMA_SEC_ITEM_DEST DMA_CTR1_DSEC
#define LL_DMA_SEC_ITEM_ALL (DMA_CTR1_SSEC | DMA_CTR1_DSEC)
#define LL_DMA_ATTR_NSEC 0U
#define LL_DMA_ATTR_SEC 1U
#define LL_DMA_ATTR_NPRIV 0U
#define LL_DMA_ATTR_PRIV 1U
/** @param channel This parameter can be a combination of the following values:
* @arg @ref LL_DMA_CHANNEL_0
* ...
* @arg @ref LL_DMA_CHANNEL_15
*/
__STATIC_INLINE void LL_DMA_SetSecAttr(DMA_TypeDef *dma, uint32_t channel, uint32_t sec_attr)
/** @param channel This parameter can be one of the following values:
* @arg @ref LL_DMA_CHANNEL_0
* ...
* @arg @ref LL_DMA_CHANNEL_15
*/
__STATIC_INLINE uint32_t LL_DMA_GetSecAttr(DMA_TypeDef *dma, uint32_t channel)
/* same for the SetPrivAttr/GetPrivAttr APIs */
__STATIC_INLINE void LL_DMA_LockAttr(DMA_TypeDef *dma, uint32_t channel)
/** @param channel This parameter can be one of the following values:
* @arg @ref LL_DMA_CHANNEL_0
* ...
* @arg @ref LL_DMA_CHANNEL_15
* @retval attribute lock status (1 or 0).
*/
__STATIC_INLINE uint32_t LL_DMA_IsLockedAttr(DMA_TypeDef *dma, uint32_t channel)
/** @param item This parameter can be a combination of the following values:
* @arg @ref LL_DMA_SEC_ITEM_SRC
* @arg @ref LL_DMA_SEC_ITEM_DEST
* @arg @ref LL_DMA_SEC_ITEM_ALL
*/
void LL_DMA_SetChannelSecAttr(DMA_ChannelTypeDef *dma, uint32_t item, uint32_t sec_attr)
/** @param item This parameter can be one of the following values:
* @arg @ref LL_DMA_SEC_ITEM_SRC
* @arg @ref LL_DMA_SEC_ITEM_DEST
*/
uint32_t LL_DMA_GetChannelSecAttr(DMA_ChannelTypeDef *dma, uint32_t item)
Note
In this Low-Layer (LL) DMA example, the attribute APIs operate as follows:
The DMA attribute APIs utilize an existing instance of type
DMA_TypeDefto set and get the security attribute for the specified channel(s).The
IsLockedAPI returns a numerical value of0or1.Two additional functions,
LL_DMA_SetChannelSecAttrandLL_DMA_GetChannelSecAttr, use an existing channel instance of typeDMA_ChannelTypeDef. These functions allow setting or retrieving the channel transfer security attribute for the itemsLL_DMA_SEC_ITEM_SRC(transfer source) andLL_DMA_SEC_ITEM_DEST(transfer destination).
HAL RIF-aware/TZ-aware peripherals APIs ¶
hal_status_t HAL_{PPP}_{SUBBLOCK}_Set{AttrName}Attr({hal_{ppp}_t instance},
{uint32_t Items/subinstances},
hal_{ppp}_{attrname}_attr_t {attrname}_attr);
hal_{ppp}_{attrname}_attr_t HAL_{PPP}_{SUBBLOCK}_Get{AttrName}Attr({hal_{ppp}_t instance},
{uint32_t Item/subinstance});
hal_status_t HAL_{PPP}_{SUBBLOCK}_Lock{AttrName}Attr({hal_{ppp}_t instance},
{uint32_t Items/subinstances});
hal_{ppp}_attr_lock_status_t HAL_{PPP}_{SUBBLOCK}_IsLocked{AttrName}Attr({hal_{ppp}_t instance},
{uint32_t Item/subinstance});
/* when the PPP HW allows to unlock the attributes */
hal_status_t HAL_{PPP}_{SUBBLOCK}_UnLock{AttrName}Attr({hal_{ppp}_t instance},
{uint32_t Items/subinstances});
With:
The
{PPP}is the HAL module name.The
{SUBBLOCK}(when existing) within a TZ-aware/RIF-aware HAL module,it must be applied within set/get attributes APIs.The
{AttrName}is the attribute abbreviation described here:Sec,Priv,Public
Instance is:
The HAL instance of type
hal_ppp_twhen existing in the given driver (e.g.hal_gpio_torhal_flash_t).Omitted when the given HAL driver does not use an instance, like HAL RCC or PWR.
Items/subinstances:
Use subinstances when the attribute applies to sub-instances, meaning multiple identical resources of the same peripheral (e.g. pins in case of GPIO). In this case, these APIs reuse the already existing instance naming and definitions (e.g. in case of GPIO, subinstances = pins and must be set to the defines
HAL_GPIO_PIN_n).Use items when the attribute applies to heterogeneous/specific parts of the given peripheral instance (e.g. the RCC oscillators and PLLs and other items). In this case, a set of dedicated defines is provided to list these items with the following naming rules:
HAL_{PPP}_{ATTRNAME}_ITEM_{ITEM}, withHAL_{PPP}_{ATTRNAME}_ITEM_ALLrequired.Omitted when the attributes apply to the given PPP instance. In this case, only the
hal_ppp_tinstance is used (e.g. HAL EXTI, where the attribute setting or lock applies to the EXTI lines represented by thehal_exti_line_tHAL instance enumeration).
Note
Set attributes APIs can be applied for one or several items/subinstances (defines can be ORed/combined when possible).
Get attributes APIs must be applied for one single item/subinstance (cannot be ORed/combined).
Lock/Unlock/IsLocked API parameters (instance, items/subinstances) must be aligned with the given device capability (whether locking can be performed at instance granularity or at item/sub-instance granularity).
The unlock function must be provided only if it is possible to unlock on the fly (i.e., without requiring a system reset).
Examples
RCC
/* Sec items list */
#define HAL_RCC_SEC_ITEM_HSE LL_RCC_SEC_ITEM_HSE
#define HAL_RCC_SEC_ITEM_LSI LL_RCC_SEC_ITEM_LSI
...
#define HAL_RCC_SEC_ITEM_SYSCLK LL_RCC_SEC_ITEM_SYSCLK
...
#define HAL_RCC_SEC_ITEM_ALL LL_RCC_SEC_ITEM_ALL
/* Priv items list */
#define HAL_RCC_PRIV_ITEM_HSE LL_RCC_PRIV_ITEM_HSE
#define HAL_RCC_PRIV_ITEM_LSI LL_RCC_PRIV_ITEM_LSI
...
#define HAL_RCC_PRIV_ITEM_PLL1 LL_RCC_PRIV_ITEM_PLL1
#define HAL_RCC_PRIV_ITEM_SYSCLK LL_RCC_PRIV_ITEM_SYSCLK
...
#define HAL_RCC_PRIV_ITEM_ALL LL_RCC_PRIV_ITEM_ALL
/* Public items list */
#define HAL_RCC_PUBLIC_ITEM_HSE LL_RCC_PUBLIC_ITEM_HSE
#define HAL_RCC_PUBLIC_ITEM_LSI LL_RCC_PUBLIC_ITEM_LSI
...
#define HAL_RCC_PUBLIC_ITEM_SYSCLK LL_RCC_PUBLIC_ITEM_SYSCLK
...
#define HAL_RCC_PUBLIC_ITEM_ALL LL_RCC_PUBLIC_ITEM_ALL
typedef enum
{
HAL_RCC_NSEC = LL_RCC_ATTR_NSEC, /*!< Non-secure access level attribute */
HAL_RCC_SEC = LL_RCC_ATTR_SEC /*!< Secure access level attribute */
} hal_rcc_sec_attr_t;
typedef enum
{
HAL_RCC_NPRIV = LL_RCC_ATTR_NPRIV, /*!< Non-privileged access level attribute */
HAL_RCC_PRIV = LL_RCC_ATTR_PRIV /*!< Privileged access level attribute */
} hal_rcc_priv_attr_t;
typedef enum
{
HAL_RCC_NPUBLIC = LL_RCC_ATTR_NPUBLIC, /*!< Non-public access level attribute */
HAL_RCC_PUBLIC = LL_RCC_ATTR_PUBLIC /*!< Public access level attribute */
} hal_rcc_public_attr_t;
typedef enum
{
HAL_RCC_ATTR_UNLOCKED = 0U,
HAL_RCC_ATTR_LOCKED = 1U
} hal_rcc_attr_lock_status_t;
hal_status_t HAL_RCC_SetSecAttr(uint32_t items, hal_rcc_sec_attr_t sec_attr);
hal_rcc_sec_attr_t HAL_RCC_GetSecAttr(uint32_t item);
hal_status_t HAL_RCC_SetPrivAttr(uint32_t items, hal_rcc_priv_attr_t priv_attr);
hal_rcc_priv_attr_t HAL_RCC_GetPrivAttr(uint32_t item);
hal_status_t HAL_RCC_SetPublicAttr(uint32_t items, hal_rcc_public_attr_t public_attr);
hal_rcc_public_attr_t HAL_RCC_GetPublicAttr(uint32_t item);
hal_status_t HAL_RCC_LockAttr(uint32_t item);
hal_rcc_attr_lock_status_t HAL_RCC_IsLockedAttr(uint32_t item);
Note
In this HAL RCC example:
The instance is omitted, as it is not used in the HAL RCC driver.
Items are used, as the attribute setting applies to heterogeneous (non-identical) parts of the RCC such as HSE, LSE, PLL1, SYSCLK.
Locking is possible per item in this example.
No unlock API is provided, as unlock is not possible (unlock is performed by a system reset).
GPIO
/* same Pin definitions used overall the HAL GPIO driver */
#define HAL_GPIO_PIN_0 LL_GPIO_PIN_0 /*!< GPIO pin 0 */
#define HAL_GPIO_PIN_1 LL_GPIO_PIN_1 /*!< GPIO pin 1 */
#define HAL_GPIO_PIN_2 LL_GPIO_PIN_2 /*!< GPIO pin 2 */
..
#define HAL_GPIO_PIN_ALL LL_GPIO_PIN_ALL /*!< GPIO pin all*/
typedef enum
{
HAL_GPIO_ATTR_NSEC = LL_GPIO_ATTR_NSEC, /*!< I/O pin is nonsecure */
HAL_GPIO_ATTR_SEC = LL_GPIO_ATTR_SEC /*!< I/O pin is secure */
} hal_gpio_sec_attr_t;
typedef enum
{
HAL_GPIO_ATTR_NPRIV = LL_GPIO_ATTR_NPRIV, /*!< I/O pin is unprivileged */
HAL_GPIO_ATTR_PRIV = LL_GPIO_ATTR_PRIV /*!< I/O pin is privileged */
} hal_gpio_priv_attr_t;
typedef enum
{
HAL_GPIO_ATTR_UNLOCKED = 0U, /*!< I/O pin attribues is unlocked */
HAL_GPIO_ATTR_LOCKED = 1U /*!< I/O pin attribues is locked */
} hal_gpio_attr_lock_status_t;
void HAL_GPIO_SetSecAttr(hal_gpio_t gpiox, uint32_t pins, hal_gpio_sec_attr_t sec_attr);
hal_gpio_sec_attr_t HAL_GPIO_GetSecAttr(hal_gpio_t gpiox, uint32_t pin);
void HAL_GPIO_SetPrivAttr(hal_gpio_t gpiox, uint32_t pins, hal_gpio_priv_attr_t priv_attr);
hal_gpio_priv_attr_t HAL_GPIO_GetPrivAttr(hal_gpio_t gpiox, uint32_t pin);
hal_status_t HAL_GPIO_LockAttr(hal_gpio_t gpiox, uint32_t pins);
hal_gpio_attr_lock_status_t HAL_GPIO_IsLockedAttr(hal_gpio_t gpiox, uint32_t pin);
Note
In this HAL GPIO example the attributes APIs use:
The
hal_gpio_tinstance: the port.The subinstances are the pins and using the same defines
HAL_GPIO_PIN_nas the overall driverThe attributes lock can be done by pin(s) in the above example.
EXTI
typedef enum
{
HAL_EXTI_NSEC = LL_EXTI_ATTR_NSEC,
HAL_EXTI_SEC = LL_EXTI_ATTR_SEC
} hal_exti_sec_attr_t;
typedef enum {
HAL_EXTI_NPRIV = LL_EXTI_ATTR_NPRIV,
HAL_EXTI_PRIV = LL_EXTI_ATTR_PRIV
} hal_exti_priv_attr_t;
typedef enum
{
HAL_EXTI_ATTR_UNLOCKED = 0U, /*!< EXTI attribues are unlocked */
HAL_EXTI_ATTR_LOCKED = 1U /*!< EXTI pin attribues are locked */
} hal_exti_attr_lock_status_t;
hal_status_t HAL_EXTI_SetSecAttr(hal_exit_line_t exit_line, hal_exti_sec_attr_t sec_attr);
hal_exti_sec_attr_t HAL_EXTI_GetSecAttr(hal_exit_line_t exit_line);
hal_status_t HAL_EXTI_SetPrivAttr(hal_exit_line_t exit_line, hal_exti_priv_attr_t priv_attr);
hal_exti_priv_attr_t HAL_EXTI_GetPrivAttr(hal_exit_line_t exit_line);
hal_status_t HAL_EXTI_LockAttr(void);
hal_exti_attr_lock_status_t HAL_EXTI_IsLockedAttr(void);
Note
In this example, the HAL EXTI attributes APIs use:
The existing instance enumeration
hal_exti_line_tas the attributes applies by lineThere are no subinstance parameter
The lock/IsLocked functions are void in the above example as the given HW EXTI peripheral allows to lock all the lines attributes together (not possible to lock individually the attributes of a given line) - In case a product allows to lock the attributes by line, then the parameter
hal_exti_line_tmust be used.NVM
/* NVM security configuration items */
#define HAL_NVM_ITF_SEC_ITEM_PM LL_NVM_SEC_ITEM_PM
..
#define HAL_NVM_ITF_SEC_ITEM_ALL LL_NVM_SEC_ITEM_ALL
/* NVM privilege configuration items */
#define HAL_NVM_ITF_PRIV_ITEM_SYS LL_NVM_PRIV_ITEM_SYS
..
#define HAL_NVM_ITF_PRIV_ITEM_ALL LL_NVM_PRIV_ITEM_ALL
/* NVM lock configuration items */
#define HAL_NVM_ITF_LOCK_ITEM_PM LL_NVM_LOCK_ITEM_PM
..
#define HAL_NVM_ITF_LOCK_ITEM_ALL LL_NVM_LOCK_ITEM_ALL
typedef enum
{
HAL_NVM_ITF_NSEC = LL_NVM_ATTR_NSEC,
HAL_NVM_ITF_SEC = LL_NVM_ATTR_SEC
} hal_nvm_itf_sec_attr_t;
/*! HAL NVM ITF Privilege attribute enumeration definition */
typedef enum
{
HAL_NVM_ITF_NPRIV = LL_NVM_ATTR_NPRIV,
HAL_NVM_ITF_PRIV = LL_NVM_ATTR_PRIV
} hal_nvm_itf_priv_attr_t;
/*! HAL NVM ITF Lock attribute enumeration definition */
typedef enum
{
HAL_NVM_ITF_ATTR_UNLOCKED = 0U,
HAL_NVM_ITF_ATTR_LOCKED = 1U
} hal_nvm_itf_attr_lock_status_t;
hal_status_t HAL_NVM_ITF_SetSecAttr(hal_nvm_t instance, uint32_t item, hal_nvm_itf_sec_attr_t sec_attr);
hal_nvm_itf_sec_attr_t HAL_NVM_ITF_GetSecAttr(hal_nvm_t instance, uint32_t item);
hal_status_t HAL_NVM_ITF_SetPrivAttr(hal_nvm_t instance, uint32_t item, hal_nvm_itf_priv_attr_t priv_attr);
hal_nvm_itf_priv_attr_t HAL_NVM_ITF_GetPrivAttr(hal_nvm_t instance, uint32_t item);
hal_status_t HAL_NVM_ITF_LockAttr(hal_nvm_t instance, uint32_t item);
hal_nvm_itf_attr_lock_status_t HAL_NVM_ITF_IsLockedAttr(hal_nvm_t instance, uint32_t item);
Note
In this HAL NVM example, the attributes APIs use:
The existing instance enumeration
hal_nvm_titems as the attributes setting applies to heterogenous parts (not identical) of the NVM
The lock/IsLocked functions use the instance enumeration
hal_nvm_tattributes and items as second parameters as the attributes lock is possible by item.DMA
typedef enum
{
HAL_DMA_NSEC = LL_DMA_ATTR_NSEC,
HAL_DMA_SEC = LL_DMA_ATTR_SEC
} hal_dma_sec_attr_t;
typedef enum {
HAL_DMA_NPRIV = LL_DMA_ATTR_NPRIV,
HAL_DMA_PRIV = LL_DMA_ATTR_PRIV
} hal_dma_priv_attr_t;
hal_status_t HAL_DMA_SetSecAttr(hal_dma_channel_t instance,
hal_dma_sec_attr_t sec_attr);
hal_dma_sec_attr_t HAL_DMA_GetSecAttr(hal_dma_channel_t instance);
hal_status_t HAL_DMA_SetPrivAttr(hal_dma_channel_t instance,
hal_dma_priv_attr_t priv_attr);
hal_dma_priv_attr_t HAL_DMA_GetPrivAttr(hal_dma_channel_t instance);
#define HAL_DMA_SEC_ITEM_SRC LL_DMA_SEC_ITEM_SRC
#define HAL_DMA_SEC_ITEM_DEST LL_DMA_SEC_ITEM_DEST
#define HAL_DMA_SEC_ITEM_ALL LL_DMA_SEC_ITEM_ALL
hal_status_t HAL_DMA_SetXferSecAttr(hal_dma_channel_t instance,
uint32_t items,
hal_dma_sec_attr_t sec_attr);
hal_dma_sec_attr_t HAL_DMA_GetXferSecAttr(hal_dma_channel_t instance, uint32_t item);
Note
In HAL DMA, there are two levels of attribute setting:
Channel attribute setting: setting the DMA channel to be used by a secure or non-secure, privileged or non-privileged context.
This is handled by the functions
HAL_DMA_SetSecAttr/HAL_DMA_GetSecAttrandHAL_DMA_SetPrivAttr/HAL_DMA_GetPrivAttr.These functions use the existing HAL DMA instance
hal_dma_channel_t. They do not use items or sub-instances.
Transfer attribute setting: setting the source/destination of a given channel transfer to be from/to a secure or non-secure area.
This is handled by the functions
HAL_DMA_SetXferSecAttr/HAL_DMA_GetXferSecAttr.These functions use the existing HAL DMA instance
hal_dma_channel_tplus anitem(s)parameter, which can be the source or the destination of the transfer.
Security compile-time conditional checks ¶
In the stm32tnxx.h CMSIS DFP file, two defines must be provided allowing to identify the current execution context secure or non-secure as follow:
//stm32tnxx.h
...
/* Cortex-M Security Extension: secure compilation */
#if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U)
#define CMSE_SECURE_EXECUTION_ENVIRONMENT
#endif /* __ARM_FEATURE_CMSE */
/* Cortex-M Security Extension: non-secure compilation */
#if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 1U)
#define CMSE_NONSECURE_EXECUTION_ENVIRONMENT
#endif /* __ARM_FEATURE_CMSE */
These defines must be used within the HAL and LL implementation as a conditional compilation switch when there is a need to differentiate between the secure and non-secure execution context.
Case of the resource/register is banked between the secure and non-secure context In this case, the corresponding registers are duplicated for secure and non-secure context. The LL and HAL drivers must provide: - A context agnostic API performing the action for the current context as follow:
__STATIC_INLINE return type LL_PPP_{SUB-BLOCK}_XXXXXXXXX(param1, param2,)
{
#if defined (CMSE_SECURE_EXECUTION_ENVIRONMENT)
STM32_SET_BIT(PPPx->secure_reg, XXXXXXXXXXXXX);
#else
STM32_SET_BIT(PPPx->nsecure_reg, XXXXXXXXXXXXX);
#endif /* CMSE_SECURE_EXECUTION_ENVIRONMENT */
}
return type HAL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
{
...
LL_PPP_{SUB-BLOCK}_XXXXXXXXX(param1, param2,)
...
}
Case of the resource/register is applicable/provided for the secure context only In this case, the corresponding HAL and LL APIs are fully delimited by the compilation define CMSE_SECURE_EXECUTION_ENVIRONMENT.
#if defined (CMSE_SECURE_EXECUTION_ENVIRONMENT)
__STATIC_INLINE return type LL_PPP_{SUB-BLOCK}NS_XXXXXXXXX(param1, param2,)
{
STM32_SET_BIT(PPPx_NS->nsecure_reg, XXXXXXXXXXXXX);
}
#endif /* CMSE_SECURE_EXECUTION_ENVIRONMENT */
#if defined (CMSE_SECURE_EXECUTION_ENVIRONMENT)
return type HAL_PPP_{SUB-BLOCK}NS_XXXXXXXX(param1, param2,)
{
...
LL_PPP_{SUB-BLOCK}NS_XXXXXXXXX(param1, param2,)
...
}
#endif /* CMSE_SECURE_EXECUTION_ENVIRONMENT */
Case of the resource/register is applicable/provided for the secure context only In this case, the corresponding HAL and LL APIs are fully delimited by the compilation define CMSE_SECURE_EXECUTION_ENVIRONMENT.
#if defined (CMSE_SECURE_EXECUTION_ENVIRONMENT)
__STATIC_INLINE return type LL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
{
MODIFY_REG(PPPx->reg, XXXXXX, xxxxx);
}
#endif /* CMSE_SECURE_EXECUTION_ENVIRONMENT */
#if defined (CMSE_SECURE_EXECUTION_ENVIRONMENT)
return type HAL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
{
...
LL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
...
}
#endif /* CMSE_SECURE_EXECUTION_ENVIRONMENT */
Case of the resource/register is applicable/provided for the non-secure context only In this case, the corresponding HAL and LL APIs are fully delimited by the compilation define CMSE_NONSECURE_EXECUTION_ENVIRONMENT.
#if defined (CMSE_NONSECURE_EXECUTION_ENVIRONMENT)
__STATIC_INLINE return type LL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
{
MODIFY_REG(PPPx->reg, XXXXXX, XXXXXX);
}
#endif /* CMSE_NONSECURE_EXECUTION_ENVIRONMENT */
#if defined (CMSE_NONSECURE_EXECUTION_ENVIRONMENT)
return type HAL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
{
...
LL_PPP_{SUB-BLOCK}_XXXXXXXX(param1, param2,)
...
}
#endif /* CMSE_NONSECURE_EXECUTION_ENVIRONMENT */
Privilege compile-time conditional checks ¶
In the
stm32tnxx.h
CMSIS DFP file, a macro must be provided allowing to identify the current execution context privilege or not as follow:
#define STM32_IS_PRIVILEGED_EXECUTION() ((__get_CONTROL() & CONTROL_nPRIV_Mask) == 0U)
Within the HAL implementation, a check must be done to check if the current privilege state allows the given action and return HAL_ERROR if not.
Example
hal_status_t HAL_RCC_SetPrivAttr(hal_rcc_priv_attr_t priv_attr)
{
if (STM32_IS_PRIVILEGED_EXECUTION() == 0U)
{
return HAL_ERROR;
}
LL_RCC_SetPrivAttr((uint32_t)priv_attr);
return HAL_OK;
}