HAL USB HCD How to Use ¶
- group HCD_How_To_Use
-
How to use the HAL USB HCD module driver ¶
Use the USB Host Controller Driver (HCD) HAL driver as follows: ¶
Declare a hal_hcd_handle_t handle structure, for example: hal_hcd_handle_t gh_hcd_usb_otg_fs;
Initialize the USB HCD low-level resources:
USB HCD interface clock configuration:
Enable USB peripheral clock.
USB HCD interface Power configuration:
Enable USB peripheral VddUSB power supply if applicable.
USB host pins configuration: USB data pins are automatically configured by the hardware during USB peripheral initialization; no additional user action is required.
NVIC configuration for interrupt handling with HAL_HCD_IRQHandler():
Set the USB HCD interrupt priority.
Enable the USB IRQ channel in the NVIC.
Initialize the USB HCD driver with HAL_HCD_Init() by selecting an instance, for example:
HAL_HCD_Init(&gh_hcd_usb_otg_fs, HAL_HCD_OTG_FS);
Declare a hal_hcd_config_t structure, for example:
hal_hcd_config_t config_hcd_usb_otg_fs;
In the configuration structure, program the PHY interface, core speed, and other parameters as required.
Apply the configuration with:
HAL_HCD_SetConfig(&gh_hcd_usb_otg_fs, &config_hcd_usb_otg_fs);
USB HCD callback definitions: ¶
By default, all callbacks are initialized to their corresponding default weak functions. When the compilation define USE_HAL_HCD_REGISTER_CALLBACKS is set to 1U, configure the driver callbacks dynamically using the callback registration functions:
Default callback weak function
Callback registration function