HAL RCC How to Use ¶
- group RCC_How_To_Use
-
This file provides firmware functions to manage the following functionalities of the Reset and Clock Control (RCC) peripheral:
Configuration and reset functions
Oscillators and Peripherals Control functions
Bus configuration functions
Main APIs are not allowed to perform any other actions than their main objective (for instance, it is not allowed to disable a PLL or an oscillator inside an enable function).
For performance reasons, few functionalities are not supported by the HAL driver but these functionalities are covered by the LL driver (for instance, interrupt management).
If the system clock is dynamically changed during runtime by the application or example code, it must call HAL_UpdateCoreClock() (a HAL generic driver function) at the end of the change to update SystemCoreClock and the systick (used by CMSIS) accordingly. The driver updates the SystemCoreClock variable and systick only in the HAL_RCC_Reset() and HAL_RCC_ResetSystemClock() functions.
¶
RCC specific features ¶
After exiting from standby or reset, the device is running from High Speed Internal (HSI) oscillator (by default at 64MHz).
There is no prescaler on High speed (AHBs) and Low speed (APBs) buses: all peripherals mapped on these buses are running at sysclk frequency.
The clock for all peripherals is switched off, except the SRAM and FLASH.
Once the device started from reset, the user application could:
Configure the clock source to be used to drive the System clock (if the application needs higher frequency/performance)
Configure the System clock frequency and Flash settings
Configure the AHB and APB buses prescalers
Enable the clock for the peripheral(s) to be used
Configure the clock source(s) for peripherals which clocks receive an independent kernel clocks.
Configure peripherals supporting the autonomous mode (These peripherals are able to generate a kernel clock request and a AHB/APB bus clock request when they need, in order to operate and update their status register even in Stop mode).