HAL SBS Overview

Introducing SBS

group SBS_Introduction

The System configuration, Boot and Security (SBS) hardware abstraction layer provides a set of APIs to interface with the STM32 SBS.

The SBS includes the following features:

  • Manage the I/O compensation cell.

  • Activate and deactivate the connection to TIM1/8/15/16/17.

  • Activate and deactivate the FPU interrupts.

  • Manage the compensation cells.

  • Manage the debug.

  • Set and get the command to be sent to the RSS executed at the next reset.

  • Get and clear the memory erase flags.

  • Get the boot address.

Module and files

The following diagram illustrates the SBS module and its associated files.

Module and files diagram

Component diagram

The following diagram illustrates the software components involved in the SBS module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.



@startuml

' The Driver name to be csutomized according to the driver
' Example CRC, I2C, NVM, FLASH, ....
!$ppp = SBS

' The HAL driver use a core driver - default value 0
!$use_ppp_core = 0

' When using a core driver : the core driver name
!$core = "XXX" + "_CORE"

' enable/disable LL RCC interfaces depandencies - default value 0
!$use_ll_rcc = 0

' the driver provide an LL layer : default value 1
' Set to 0 if core is set to 1
!if ($use_ppp_core == 1)
!$use_ppp_ll = 0
!else
!$use_ppp_ll = 1
!endif
' the driver provide a HAL Layer : default value 1
!$use_ppp_hal = 1

' the HAL driver use HAL services : default value 1
!$use_hal_service = 0

' the HAL driver use HAL RCC services : default value 1
!$use_hal_rcc = 0

' the HAL driver use HAL DMA services : default value 1
!$use_hal_dma = 0

' The driver use HAL_RCC_PPP_GetClockFreq()
!$use_kernel_clock = 1

' HAL driver use depandencies with generic instead of interfaces
!$use_hal_generic_dep = 0

' The driver use interrupts : default value 1
' Example CCB -->  no interrupts
!$use_ppp_isr = 1

' The driver use an extended file : default value 0
' Example of Usage NVM, FLASH
!$use_hal_ppp_extend = 0

' The HAL Driver extension name
!$ppp_extend = "EXT"

' The HAL Driver interface
!$hal_api_itf = "HAL " + $ppp + " API"

' The HAL Driver extended interface
!$hal_api_ext_itf = "HAL " + $ppp + " " + $ppp_extend + " API"

' The Use Application Interface
!$appli_itf = $ppp+ " User Callback"
!$appli_ext_itf = "\n" + $ppp+ " " + $ppp_extend + " User Callback"

' The HAL PPP name
!$ppp_name = "HAL_" + $ppp
!$ppp_ext_name = "HAL_" + $ppp+ "_" + $ppp_extend

' The PPP isr
!$ppp_ISR  = $ppp + " ISR"
!$ppp_ext_ISR = $ppp+ " " + $ppp_extend + " ISR"

' The LL Driver name
!$ll_ppp   = "LL_" + $ppp

!$hal_dma_itf = "HAL_DMA_StartDirectXfer_IT_Opt()\nHAL_DMA_Abort_IT"
!if ($use_kernel_clock == 1)
!$hal_rcc_itf = "\t\t\tHAL_RCC_"+$ppp+"_GetClockFreq()\n\t\t\tHAL_RCC_"+$ppp+"_EnableClock()"
!else
!$hal_rcc_itf = "\t\t\tHAL_RCC_"+$ppp+"_EnableClock()"
!endif

!$hal_ppp_itf = "Half transfer complete\nTransfer complete\nError callback\nAbort callback"

' HAL Generic interface for the PPP driver
!$hal_generic_itf = "HAL_GetTick()"

!$ll_ppp_itf = "LL " + $ppp +" API"

' HW
!$ppp_xIRQ = $ppp+"x_IRQ"


<style>
componentDiagram {
   arrow {
      FontSize 8
   }
   interface {
      FontSize 8
   }
}
</style>

title $ppp Software Component Diagram

Package "Application Layer" {

  component [Appli]
  !if ($use_ppp_isr == 1)
  interface "$appli_itf" as APPLI_Interface
  [Appli] -r- APPLI_Interface
  !if ($use_hal_ppp_extend == 1)
  interface "$appli_ext_itf" as APPLI_EXT_Interface
  [Appli] -l- APPLI_EXT_Interface
  !endif
  !endif
}

package "HAL" {
    !if ($use_hal_ppp_extend == 1)
    [$ppp_name]
    [$ppp_ext_name]
    !else
    [$ppp_name]
    !endif
    !if ($use_hal_dma == 1)
      interface "$hal_ppp_itf" as HAL_PPP_Interface
      [$ppp_name] -d- HAL_PPP_Interface
    !endif
    interface "$hal_api_itf" as HAL_PPP_APPLI_Interface
    !if ($use_hal_ppp_extend == 1)
    interface "$hal_api_ext_itf" as HAL_PPP_APPLI_EXT_Interface
    [$ppp_name] -u- HAL_PPP_APPLI_Interface
    [$ppp_ext_name] -u- HAL_PPP_APPLI_EXT_Interface
    '[$ppp_ext_name] -u-(
    [$ppp_name] ..> [$ppp_ext_name] : <<include>>
    !else
    [$ppp_name] -u- HAL_PPP_APPLI_Interface
    !endif
    !if ($use_hal_generic_dep == 0)
      !if ($use_hal_service == 1)
        [HAL_SERVICE]
        interface "$hal_generic_itf" as HAL_Service_Interface
        [HAL_SERVICE] -r- HAL_Service_Interface
        [$ppp_name] -l-( HAL_Service_Interface
        !if ($use_hal_ppp_extend == 1)
          [$ppp_ext_name] -r-( HAL_Service_Interface
        !endif
      !endif
    !else
          [HAL_SERVICE]
          [$ppp_name] ..> [HAL_SERVICE]
    !endif
    !if ($use_hal_dma == 1)
      [HAL_DMA]
      interface "$hal_dma_itf" as HAL_DMA_Interface
      [HAL_DMA] -u- HAL_DMA_Interface
      [HAL_DMA] -u-( HAL_PPP_Interface
      [$ppp_name] --( HAL_DMA_Interface
    !endif
    !if ($use_hal_rcc == 1)
      [HAL_RCC]
      interface "$hal_rcc_itf" as HAL_RCC_Interface
      [HAL_RCC] -l- HAL_RCC_Interface
      [$ppp_name] -r-( HAL_RCC_Interface
    !endif

}

[Appli] -d-( HAL_PPP_APPLI_Interface
!if ($use_hal_ppp_extend == 1)
[Appli] -d-( HAL_PPP_APPLI_EXT_Interface
!endif
!if ($use_ppp_isr == 1)
[$ppp_name] -u-( APPLI_Interface
!if ($use_hal_ppp_extend == 1)
[$ppp_ext_name] -u-( APPLI_EXT_Interface
!endif
!endif
!if ($use_ppp_core ==1)
Package "Core Layer" {
    [$core]
    interface "core API" as Core_api_itf
    [$core] -u- Core_api_itf
}
[$ppp_name] -d-( Core_api_itf
!endif
package "Low Layer" {
    [CMSIS-Devices]
    !if ($use_ppp_ll == 1)
      [$ll_ppp]
      interface "$ll_ppp_itf" as LL_PPP_Interface
      [$ll_ppp]  -u- LL_PPP_Interface
    !endif

    !if ($use_ppp_isr == 1)
    interface "$ppp_ISR" as PPP_ISR
    [$ppp_ISR] -u- PPP_ISR
    [$ppp_ISR]
    !if ($use_hal_ppp_extend == 1)
      interface "$ppp_ext_ISR" as PPP_EXT_ISR
      [$ppp_ISR] -u- PPP_EXT_ISR
      [$ppp_ext_name] -d-( PPP_EXT_ISR
    !endif
    !endif



    !if ($use_ll_rcc == 1)
      [LL_RCC]
      interface "LL RCC API" as LL_RCC_API
      [LL_RCC] -u- LL_RCC_API
      [HAL_RCC] -d-(LL_RCC_API
    !endif

    !if ($use_hal_dma == 1)
      [DMA ISR]
      interface "DMA ISR" as DMA_ISR
      [DMA ISR] -u- DMA_ISR
    !endif

}

package "HW" {
    [STM32_HW]
    !if ($use_ppp_isr == 1)
      interface "$ppp_xIRQ" as PPPx_IRQ
      [STM32_HW] -u- PPPx_IRQ
    !endif
    !if ($use_hal_dma == 1)
      interface "DMAx_IRQ_Ch" as DMA_IRQ_CH
      [STM32_HW] -u- DMA_IRQ_CH
      [DMA ISR] -d-( DMA_IRQ_CH
      [HAL_DMA] --( DMA_ISR
    !endif
}
!if ($use_ppp_ll == 1)
    !if ($use_hal_ppp_extend == 1)
      [$ppp_ext_name] -d-( LL_PPP_Interface
    !else
      [$ppp_name] -d-( LL_PPP_Interface
    !endif
    [$ll_ppp] .r.> [CMSIS-Devices]: $ppp register def
    [STM32_HW] <.u. [$ll_ppp] : $ppp registers R/W
!else
    !if ($use_ppp_core == 1)
      [$core] .l.> [CMSIS-Devices]: $ppp register def
      [STM32_HW] <.u. [$core] : $ppp registers R/W
    !else
      [$ppp_name] .d.> [CMSIS-Devices]: $ppp register def
      [STM32_HW] <.l. [$ppp_name] : $ppp registers R/W
    !endif
!endif
!if ($use_ppp_isr == 1)
   [$ppp_ISR] -d-( PPPx_IRQ
   [$ppp_name] -d-( PPP_ISR
!endif
!if ($use_ll_rcc == 1)
   [STM32_HW] <.u. [LL_RCC] : RCC registers R/W
!endif


@enduml

Configuration table

The following table lists the configuration defines for the HAL SBS module, specifying their locations, default values, and descriptions:

group SBS_Configuration_Table

Configuration inside the SBS driver

Config defines

Description

Default value

Note

USE_HAL_SBS_MODULE

from hal_conf.h

1U

When set to 1, the HAL SBS module is enabled.

USE_ASSERT_DBG_PARAM

from IDE

None

When defined, enable the params assert.