Community ¶
Support link ¶
If you need assistance or have questions regarding STM32CubeProgrammer, support is available. Access a wide range of resources and receive help from the STMicroelectronics support team.
For more information and to get support, visit the STMicroelectronics Support Home.
Community link ¶
Feedback is valuable and helps improve STM32CubeProgrammer. If you have suggestions, issues, or comments, share them with the community.
To provide feedback and participate in discussions, visit the ST Community.
Knowledge articles link ¶
To find information on STM32 microcontroller programming, troubleshooting, ecosystem, and product details, visit the STM32 MCUs Knowledge Base.
Additional links ¶
ST-Link connect
STM32U5, RDP regression with password and TrustZone
How to disable Trustzone on STM32U5 Series - STMicroelectronics Community
How to regress from RDP level 2 to RDP level 0 on the STM32U5 series - STMicroelectronics Community
Precautions to avoid lock states when developing with TrustZone - STMicroelectronics Community
STM32H5, product state and DA
How to enable RDP-like product state flash protection in STM32H5 - STMicroelectronics Community
Implementing debug authentication on STM32H5 using CLI tools - STMicroelectronics Community
STM32H7
BL/OpenBL
Factory reset
Reg dump
External loaders
STM32N6
How to add the STM32N6’s header signature as post build output - STMicroelectronics Community
How to connect the STM32N6 using STLINK and serial boot interfaces - STMicroelectronics Community
How to create an STM32N6 FSBL load and run - STMicroelectronics Community
How to program the OTP fuse bits in the STM32N6 - STMicroelectronics Community