Import/Export project settings

The user can load or store the settings below from or to a .prog project file:

  • Connection settings, only if the board is connected.

  • Firmware’s list.

  • External flash loaders.

  • Settings used for the automatic mode.

  • Settings of STM32WB stack install, only when connecting STM32WB devices.

  • RSSe binaries.

  • Option bytes values, only if the board is connected.

To import the settings, choose the settings file path and check at least one option.

Note

Import settings interface illustration is not available in this repository snapshot.

If the device ID saved in the imported project settings does not match the connected device, a warning message appears.

After importing the option bytes settings from the Import/Export Settings tab, apply them from the Option Bytes tab by clicking the Take OB from Project Settings button.

To export the settings, choose at least one option.