Main window MPUs

../../../_images/Main_window_MPUS-Fig141.webp

Fig. 93 STM32CubeProgrammer main window

The main window allows the user to select the interface used to connect to STM32MPxx BootROM. Possible interfaces are USB-DFU and UART, since programming through STLink interface is not possible with STM32MPxx devices.

Once connected using the Connect button, available partitions are displayed, and the user is able to open a TSV file for programming.