Comparison between two files ¶
Description: compares the content of two different files, binary, hex, srec, elf, out, and axf. The difference is colored in red in the grid panel of each file.
This operation does not need a connected board.
The used files can be of different sizes and types.
The user can open the comparison window from different sub-menus.
Fig. 83 Sub-menu displayed from Read combo-box in device memory tab ¶
Fig. 84 Sub-menu displayed with right click on Device memory tab ¶
Fig. 85 Sub-menu displayed with right click on the cell of grid ¶
Fig. 86 Sub-menu displayed with add tab button ¶
Fig. 87 Sub-menu displayed with right click on the opened file tab ¶
Fig. 88 Sub-menu displayed from Download combo-box displayed in file tab ¶
Note
In addition to sub-menus to display this window, the user can open it directly by using the key combination Ctrl+F.
Example: Difference between two files of the same type and different sizes ¶
Fig. 89 Data width: 32 bits ¶
Fig. 90 Data width: 16 bits ¶
Fig. 91 Data width: 8 bits ¶
Note
The user can make multiple comparisons between files.
Fig. 92 Multiple comparisons ¶