HAL I2S Overview ¶
Introducing I2S ¶
- group I2S_Introduction
-
The I2S hardware abstraction layer provides a set of APIs to interface with the STM32 I2S (Inter-integrated circuit sound) peripheral.
It simplifies the configuration, initialization, and management of I2S communication by supporting various modes such as polling, interrupt, and DMA for efficient data transfer.
This abstraction layer ensures portability and ease of use across different STM32 series.
Module and files ¶
The following diagram illustrates the I2S module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the I2S module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL I2S module, specifying their locations, default values, and descriptions:
- group I2S_Configuration_Table
-
¶
Configuration inside the I2S driver ¶
Software configuration defined in stm32c5xx_hal_conf.h:
Preprocessor flags
Default value
Comment
USE_HAL_I2S_MODULE
1
Enable the HAL I2S driver module
USE_HAL_I2S_REGISTER_CALLBACKS
0
Allow an application to define a callback
USE_HAL_I2S_DMA
1
Enable the DMA code inside I2S
USE_HAL_CHECK_PARAM
0
Enable runtime parameter check
USE_HAL_I2S_CLK_ENABLE_MODEL
HAL_CLK_ENABLE_NO
Enable the gating of the peripheral clock
USE_HAL_MUTEX
0
Enable semaphore creation for OS
USE_HAL_I2S_USER_DATA
0
Add user data inside the HAL I2S handle
USE_HAL_I2S_GET_LAST_ERRORS
0
Enable retrieving last process error codes
USE_HAL_I2S_OVR_UDR_ERRORS
0
Enable retrieving overrun and underrun errors
Software configuration defined in preprocessor environment:
Preprocessor flags
Default value
Comment
USE_ASSERT_DBG_PARAM
Not defined
Enable parameter check for HAL and LL
USE_ASSERT_DBG_STATE
Not defined
Enable state check for HAL