HAL SPI Overview ¶
Introducing SPI ¶
- group SPI_Introduction
-
The SPI hardware abstraction layer provides a set of APIs to interface with the STM32 SPI (Serial Peripheral Interface) peripheral.
It simplifies the configuration, initialization, and management of SPI communication, by supporting various modes such as polling, interrupt, and DMA for efficient data transfer.
This abstraction layer ensures portability and ease of use across different STM32 series.
Module and files ¶
The following diagram illustrates the SPI module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the SPI module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL SPI module, specifying their locations, default values, and descriptions:
- group SPI_Configuration_Table
-
¶
Configuration inside the SPI driver: ¶
Software configuration defined in stm32c5xx_hal_conf.h:
Preprocessor flags
Default value
Comment
USE_HAL_SPI_MODULE
1
Enable HAL SPI driver module
USE_HAL_SPI_REGISTER_CALLBACKS
0
Allow the user to define their own callback
USE_HAL_SPI_DMA
1
Enable DMA code inside SPI
USE_HAL_CHECK_PARAM
0
Enable runtime parameter check
USE_HAL_SPI_CLK_ENABLE_MODEL
HAL_CLK_ENABLE_NO
Enable the gating of the peripheral clock
USE_HAL_CHECK_PROCESS_STATE
0
Enable atomicity of process state check
USE_HAL_MUTEX
0
Enable semaphore creation for OS
USE_HAL_SPI_USER_DATA
0
Add a user data inside HAL SPI handle
USE_HAL_SPI_GET_LAST_ERRORS
0
Enable retrieval of last processes error codes
USE_HAL_SPI_CRC
1
Enable the use of CRC feature inside driver
Software configuration defined in preprocessor environment:
Preprocessor flags
Default value
Comment
USE_ASSERT_DBG_PARAM
Not defined
Enable check param for HAL and LL
USE_ASSERT_DBG_STATE
Not defined
Enable check state for HAL